You are here: Understanding KAS > Motion Concepts > Pipe Network Concept

Pipe Network Concept

To introduce the Pipe Network concept, we can use a mechanical analogy.

In the figure below, the mechanical system is composed of three-axes and driven by one motor. All axes are connected to the motor through shafts, gears and cams. When the motor is in motion, all axes are moving synchronously. The speed relation between the Master and the Axis is achieved by using a mechanical Gear. A mechanical cam is used to get linear motion from a rotating wheel.

Figure 5-6: Mechanical System

The Pipe Network in the figure below corresponds to the mechanical system described above. The pipe concept is a one-to-one translation of a mechanical system into the logical world.

Pipe Network Structure

Figure 5-7: Pipe Network Structure

In our Pipe Network, the analogy is as follows:

The Pipe Network concept allows motion engineers to define in a very natural way the physical relationships between the different axes of their machine.

This powerful modular approach provides a solution for almost any multi-axis requirements. It also remains open for new, additional functions that can be required in the future.

Concept Link IconSee Also

 

Pipe Network

Pipe Structure

Pipe Block

Axis Pipe Block

Executing Motion

Pipe Block Lifetime

Motion State Machine

Phase Execution in the Pipe Network

Use Motion Function Block

Function - General rules


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™